2020-10-19 07:50 AM
Hi,
I am using a SPC570S-DISP development board, and I am trying to create a new application form that. I have tested out a few example application given in the IDE, and they work fine.
Now I want to develop such an application from scratch. However, there seem to be no guide as such, showing the necessary step to follow in order to properly configure the application. I have also referred the Help section.
One problem that I came across is that, in the MCU wizard, I am unable to configure any of the peripherals. When I click on one of the peripherals, no options seem to appear. Is there a document that can be referred, or a tutorial that I can follow?
Thanks.
Dinuke
Solved! Go to Solution.
2020-10-21 02:30 AM
1) First, add the platform component
2) You have to click on the + button to add the compatible component
Best regards
Erwan
2020-10-20 07:54 AM
Hello Dinuke ,
There is a help section in SPC5Studio , (Cf Help Section)
you can add any compatible component, configure and generate the code.
Best Regards
Erwan
2020-10-20 09:16 AM
Hello Erwan,
I followed the help section. I have already created a new SPC5Studion application. I cant unable to find compatible components. Where do I can find the compatible components.
Best Regards,
Dinuke
2020-10-21 02:30 AM
1) First, add the platform component
2) You have to click on the + button to add the compatible component
Best regards
Erwan