Hi ST Community,
I'm working on a project using the SPC58EC80E microcontroller on the SPC58EC-DISP board.
I'm particularly interested in optimizing the configuration of the two cores (e200z420n3) and understanding their inter-core communication mechanisms.
Specific Questions:
Core Configuration:
- What is the most efficient way to configure the two cores for optimal performance?
- What factors should be considered when determining the core clock frequencies and priorities?
Inter-Core Communication:
- How can I effectively implement inter-core communication between the two cores?
- Are there specific mechanisms or protocols recommended for this purpose?
- How can I ensure synchronization and data consistency between the cores?
FreeRTOS Usage:
- Can I utilize FreeRTOS on both cores simultaneously?
- If so, what considerations should be made for task scheduling, resource sharing, and inter-core communication?
- How can I configure the FreeRTOS kernel to take advantage of the dual-core architecture?
Core Process stack Size, IRQ Stack Size and load address:
![mmansouri_0-1730296978407.png mmansouri_0-1730296978407.png](https://community.st.com/t5/image/serverpage/image-id/91860iE59D0732340696E4/image-dimensions/581x260/is-moderation-mode/true?v=v2)
- What is the significance of the "Process stack Size" and "IRQ Stack Size" parameters?
- How do these parameters affect the performance and memory usage of the core?
- What are the recommended values for these parameters in different use cases?
- What is the purpose of the "Load Address" parameter?
- How does it influence the memory mapping and code execution of a process or task?
- How should this parameter be set to ensure correct execution and avoid memory conflicts?
I would be grateful for any insights, code examples, or best practices that can help me optimize the performance and reliability of my application.