2023-09-05 08:24 AM
hello everyone, i'd like to know if i can use the EVALSTDRIVE101 add-on board driven by an stm32-nucleo to drive BLAC motors. Because the datasheet says that they are suitable for BLDC AND PMSM.
Otherwise there is some other board that allows driving blac motors?
Solved! Go to Solution.
2023-09-05 08:58 AM - edited 2023-09-05 08:58 AM
STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.
Best regards.
II
2023-09-05 08:33 AM - edited 2023-09-05 08:46 AM
Hello @Nicholas_minafra97
As you can see in this description
The EVALSTDRIVE101 is designed to drive three-phase brushless DC motors.
That's why it can't drive BLAC motors.
For AC motors driver, I suggest you to take a look at this .
Best regards.
II
2023-09-05 08:49 AM
hello, @Issamos
Can you tell me if STEVAL-IPM15B can be driven by a stm32-nucleo and if it can drive a BLAC motor ?
thank you.
2023-09-05 08:58 AM - edited 2023-09-05 08:58 AM
STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.
Best regards.
II