2023-02-13 12:03 AM
I am using spc5studio and SPC58EC80E1.
i import crc sample from application library.
i set CRC Settings at low level Drivers component RLA
- CRC-32, Polymonial seed 0x4c11db7, reset = 0xFFFFFFFF
and firmware code
-----------------------------------------------------------------------------------------------------
const CRCContextConfig *crc_ctx_config[] = {
&crc_context_config_contex_crc32,
};
(void)crc_lld_start(&CRCD1);
(void)crc_lld_start_context(&CRCD1, 0, crc_ctx_config[0]);
if (crc_lld_calc(&CRCD1, 0, startAddress, (uint32_t)length, &calculatedCRC) != CRC_NO_ERROR) {
osalThreadDelayMilliseconds(100);
}
(void)crc_lld_stop_context(&CRCD1, 0);
(void)crc_lld_stop(&CRCD1);
-----------------------------------------------------------------------------
The code for the window is as follows.
uint Polynominal = 0x04C11DB7;
uint InitValue = 0xFFFFFFFF;
int i= 0, j = 0;
uint CRC = 0xFFFFFFFF;// InitValue;
for (i = 0; i < nByte; i++)
{
byte ch = c[i];
for (j = 0; j < 8; j++)
{
CRC = (uint)(ch ^ CRC);
if ((CRC & 0x80000000) != 0)
{
CRC = (CRC <<1) ^ Polynominal;
}
else
{
CRC <<= 1;
}
}
}
---------------------------------------------------------------------------------
later
I checked crc value the image of flash, but it is different from the CRC-32 calculation in windows program.
I want to know how to calculate the application library.
Or, I would appreciate it if you could let me know if my code is wrong.
thanks.
regards.
Solved! Go to Solution.
2023-02-13 7:49 AM
Hello ,
Interesting issue ;)
Could you try your software code in SPC58EC ?
Could you check this application SPC560Pxx OS-Less CRC Test Application for Discovery
there is a CRC calculation SW.
Best regards
Erwan
2023-02-13 7:49 AM
Hello ,
Interesting issue ;)
Could you try your software code in SPC58EC ?
Could you check this application SPC560Pxx OS-Less CRC Test Application for Discovery
there is a CRC calculation SW.
Best regards
Erwan
2023-02-13 6:08 PM
hello.
thanks for your answer.
i already used SPC58ECxx_RLA CRC Test Application for Discovery.(the same SPC560Pxx OS-less....)
Firmware has already applied the above code to create the CRC.
i should compare the two by making CRC in the window program with the same image.
I'm inquiring because these two crc values are different.
best regards.
Pil
2023-02-13 6:35 PM
For left shifting you'd need to get the data into the high order bits, surely?
CRC = ((uint)(ch) << 24) ^ CRC;
CRC are very sensitive to exact bit order, byte ordering, shift direction, etc.
If you've got anything wrong, you'll get different numbers, so pay particular attention to the details.