2023-07-01 9:30 PM
Hi,
I am trying to communicate with BMS IC on our developed board and I donot see the communication happening with BMS IC despite of following all the instructions
I have a L9963E BMS Eval board for reference,
I have tapped out the SPI frames on the bus to see the data
I could see for the 5 byte of frame data 4 bytes are going first and 2 byte is going after a delay of around 2.2 us
when I have fed the SPI API spi_lld_exchange with 5 bytes the data goes out in one after the other continously
Is there any specific reason why the data is send in this way?
I do not see any specific section mentioning any where in L9963E data sheet regarding this?
Kindly let me know what could be the reason for this do I need to send the data in this way?
Also I could see the clock frequency is varying in between 8MHz and 12MHz if see the clock in the image it is not pulsated at same frequency
2023-09-01 1:22 AM
Hello ,
sorry for the delay.
Did you solve your issue?
Do you RLA drivers SPI ?
Best regards
Erwan
2023-10-18 11:27 PM
did you solved that issue .
How you developed that spi communication from externel mcu ?
2023-11-19 8:43 AM
if you are using an SPC5 microcontroller you can refer to the BMS example in AutoDevKit by importing existing example. You can then compare with your code.