2024-10-16 12:35 AM - edited 2024-10-16 2:17 AM
Dear Community members,
I have connected 2 node in ring configuration, and working on an custom pcb for BMS.
In registers Faults1, Fault_L_line_status is always 1, while all other fields of Faults1 and Faults2 registers are 0.
Also the OVRLATCH is not detected.
What could be cause to set 'Fault_L_line_status' 1 and where could I check to diagnose.
screenshot for expression view is added for reference for both nodes 1 and 2.
Regards,
bitBuddy
2024-10-16 10:43 AM
Hi,
Let's exclude that you have an electrical issue.
There are several conditions triggering the Fault_L even without the OVRLATCH = 1. These conditions are reported in page 76 of the datasheet.
In the latest version of the BMS driver present in AutoDevKit, we have added a specific structure for the purpose of this check: AEK_POW_BMS63CHAIN_fastDiag_t
Here you are the function call:
AEK_POW_BMS63CHAIN_fastDiag_t AEK_POW_BMS63CHAIN_node_getFastDiag(AEK_POW_BMS63CHAIN_chain_name_t AEK_POW_BMS63CHAIN_chain_name, AEK_POW_BMS63CHAIN_node_devName_t AEK_POW_BMS63CHAIN_node_devName);
Best Regards,
AutoDevKit Team
2024-10-18 9:45 PM
Hi Max,
In L9963E data sheet, in Table 21 MISO2 where frame no. is 2 (0b10), is this referring to burst response frame no. 1 in Table 24, 25, 26 ?
2024-10-22 1:47 AM
Hi,
The answer is Yes.
Best Regards,
AutoDevKit Team
2024-10-22 10:12 PM
Hi Max,
seems it is a documentation error.
with regards,
bitBuddy
2024-10-25 1:35 AM
Hi,
There is one more message described in the miso1 row.
Best Regards,
AutoDevKit Team
2024-11-07 12:46 AM - edited 2024-11-07 12:47 AM
Hi Max,
As per observation in logic analyser, in burst(0x78) command feedback frame(MISO1 in table 21), data field is for frame 1 of Table.24 and burst response frame MISO2(in table 21) where frame no. is 2 (0b10) referring to frame 2 of table 24.
Hence we get max of 18 frame (MISO18 : Frame Num-18 (10010) in table 21) .
Regards,
bitBuddy