2024-01-12 06:46 AM
Hi,
Im working on a project which need using a op-amp and a comparator. In that matter I’ve looked at the tsv6395 which have great spec as an op-amp, but i wonder if it is acceptable to use one channel as comparator?
the signal is about 100hz
Thanks for any advice,
Mg
Solved! Go to Solution.
2024-01-12 08:23 AM
Hi,
I see no problem - same, as with any other dual opamp.
Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.
2024-01-12 08:23 AM
Hi,
I see no problem - same, as with any other dual opamp.
Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.
2024-01-12 10:10 AM
Thank you!
I just wanted to confirm as I can see that some manufacturers spec both for and against for some of their amplifiers.
best regards,
Mg