cancel
Showing results for 
Search instead for 
Did you mean: 

Tsv6395

Bratland
Associate

Hi, 

Im working on a project which need using a op-amp and a comparator. In that matter I’ve looked at the tsv6395 which have great spec as an op-amp, but i wonder if it is acceptable to use one channel as comparator? 

the signal is about 100hz

Thanks for any advice,

Mg

 

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

Hi,

I see no problem - same, as with any other dual opamp.

Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Chief III

Hi,

I see no problem - same, as with any other dual opamp.

Just they are not "fast" as comparator, 0,7V/us slew, about 4us switching time ; if this is enough for you , then ok.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you!

I just wanted to confirm as I can see that some manufacturers spec both for and against for some of their amplifiers. 

best regards,

Mg