cancel
Showing results for 
Search instead for 
Did you mean: 

TDA7498MV EPU Up or Down?

furuno
Associate
Posted on August 28, 2014 at 11:35

Hi,

I am planning to use TDA7498MV for Active Speaker application.

According to Datasheet Rev4, I am confusing about package. I need a EPU type package because of big out-put power. Description and Table-1 said EPU,however illustration and Fig-26 show EPD. Which is correct? Please confirm.

Best Regard

Hiroshi Furuno
1 REPLY 1
Nickname1623_O
Associate II
Posted on August 28, 2014 at 11:54

hi Hiroshi ,

in fact TDA7498MV is EPU type , the thermal pad is on the top of device , due to the dissipation power is much higher when the output power is reach 100W , so an external heat sink must be added to cool down the device and maintaion rated output power .

thanks

From: furuno.hiroshi

Posted: Thursday, August 28, 2014 11:35 AM

Subject: TDA7498MV EPU Up or Down?

Hi,

I am planning to use TDA7498MV for Active Speaker application.

According to Datasheet Rev4, I am confusing about package. I need a EPU type package because of big out-put power. Description and Table-1 said EPU,however illustration and Fig-26 show EPD. Which is correct? Please confirm.

Best Regard

Hiroshi Furuno