2018-03-02 2:13 AM
Hello, team.
My customer is using STPA003CD-48X and developing new H/W.
In the datasheet (5.3.1 Short circuits and open circuit operation),
>In case of short circuit to ground or Vcc, the amplifier exits from the three-state condition
>only when the output returns inside the limits imposed by an internal voltage comparator.
Could you please explain more details like concrete method to detect the short?
>When a short across the load is present, the power stage sees an over-current and is
>brought in protection mode for 100 ?s.
What is the threshold current to detect the short?
Regards, Kurosawa
#stpa003cd-48x2018-04-16 1:49 AM
Hello Kurosawa,
If short to Vcc or Gnd, the overcurrent will trigeer the protection. This protection will latch until the output level is between Vcc/2+2V and Vcc/2-2V.
For the across load short, the threshold of overcurrent is not a constant value, it depends on the Vds of the power MOS. Normally, on the STPA003 it ranges from about 3.5A to 11A
Regards,
Mauro