cancel
Showing results for 
Search instead for 
Did you mean: 

STA350BW Power Supply

joern23
Associate
Posted on August 06, 2013 at 12:50

Hi

i want to use the STA350BW amplifier but i am not quite sure which power supply i must use.

The first page of the Datasheet says:

Four power output configurations(a)

– 2 channels of ternary PWM (stereo mode)

(2 x 50 W into 6 Ω at 25 V)

– 3 channels - left, right using binary and LFE

using ternary PWM (2.1 mode) (2 x 18 W +

1 x 40W into 2 x 4 Ω, 1 x 8 Ω at 25 V)

– 2 channels of ternary PWM (2 x 50 W) +

stereo lineout ternary

– 1 channel of ternary PWM as mono-

The specifications page says:

Continuous output power, BTL, ternary mode

THD = 1% 27 W

THD = 10% 36 W

Continuous output power SE, binary mode, RL = 4 Ω

THD = 1% 12 W

THD = 10% 15.5 W

What kind of power supply will be sufficient?

Do i need something around 50 W with peak power over 100 W

or must i go up to 100 W continuous power with more peak?

Is the info from the first page related to music power or something similar?

thx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nickname14663_O
Associate II
Posted on February 14, 2014 at 13:18

Hello Harry,

This forum is dedicated to operational amplifiers, comparators and current sensing products.

In order to be more efficient with appropriate answers, another e2e forum has been created for audio amplifiers.

In order to have an accurate answer by our audio support team, would it be possible to copy/paste your question to the related forum please ?

Here is the hyperlink shortcut :

https://my.st.com/public/STe2ecommunities/analog/Lists/Audio%20Amplifiers/AllItems.aspx

Sorry for the inconvenience.

Best regards,

Sylvain

Nickname1623_O
Associate II
Posted on February 18, 2014 at 03:18

Hi Harry,

the supply power is relevant with your target output power,output configuration and test method .normally for STA350BW  50W x2 output configuration, a 60W power supply is enough  for music .

the first page info are STA350BW max output power  and continous output power that had been limited by thermal impedance of PCB , for higher continous output power , a slug up package version STA350B is available now , it can deliver mentioned max outptu power with suitable external heak sink.

Thanks .