cancel
Showing results for 
Search instead for 
Did you mean: 

SPC582B flashing error

MohitManvar
Associate II

hello team,

I'm using AutodevKit studio for testing AEK_AUD_C1D9031 board.

I imported example code from sample : SPC582Bxx_RLA_AEK_AUD_C1D9031 - Avas Compact - Test Application.

 


but upon flashing board I'm getting this error.

MohitManvar_0-1725527788326.png


kindly provide feedback. for your reference I'm attaching log file.

Mohit M

5 REPLIES 5
ATROI
ST Employee

 

Hi MohitManvar,

Please could you try to clean and rebuild the project and then try to flash it again.

Thanks, 

AutoDevKit Team

Hello,

i tried with that but not working. even I tried to re import sample project but that is also not working

Hi,

Please make sure that the board is properly connected with cable working and that it is recognized by UDE (if you are using PLS...).

Best Regards,

AutoDevKit Team

I checked connections and also able to flash from other workspace.
it is not connection issue. kindly help for ws debug launch settings.

below are current configurations.

MohitManvar_0-1725623369349.png

MohitManvar_1-1725623386806.png

suggest if anything wrong in this.

Mohit M :)

ATROI
ST Employee

Hi MohitManvar,

When you wrote "I am able to flash from other workspace",
does it mean that you're able to flash another project in the same AEK board or different AEK board?
Other things, can you post us the screen shots of the tabs:
Main and SVD Path tabs of the Debug configuration?

 

Thanks,

AutoDevKit Team