cancel
Showing results for 
Search instead for 
Did you mean: 

Powering multiple optical front-ends

Pavel_47
Associate II

Hello,

There are 8 optical front-ends on the board ... the front-ends based on TSV771 (or TSV772, TSV782, TSV791, TSV792).

Is it important to use one LDO per front-end or powering all 8 frontends by a single LDO will be also Ok ?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

As I said, I don't know the circuit or the necessary parameters, but I assume that ferrite beads could be a bit scarce because their inductance is usually quite small. Perhaps a simulation or a test could be useful.

For the capacitors, MLCCs might be the best choice.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

Even if the opamps are used as transimpedance amplifiers, separate LDOs are not necessarily an advantage because their PSRR and its frequency dependence play a major role and should also be taken into account. Without knowing your application in detail, it might make sense in your case to use a single LDO and separate the supply voltages of the individual opamps cleanly with LC filters and a carefully designed layout including GND.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel_47
Associate II

Hi Peter

Thanks. Considering that the PSRR is quite high at low frequencies and damps at high frequencies, perhaps ferrite beads would be sufficient to separate the VDDs of OpAmps ?

Peter BENSCH
ST Employee

As I said, I don't know the circuit or the necessary parameters, but I assume that ferrite beads could be a bit scarce because their inductance is usually quite small. Perhaps a simulation or a test could be useful.

For the capacitors, MLCCs might be the best choice.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel_47
Associate II

Ok, thanks Peter.