cancel
Showing results for 
Search instead for 
Did you mean: 

Is TS912AIDT opamp unity gain stable? If not can we make this opamp unity gain stable using external circuitary or by any other way? If not can you propose unity gain stable opamp which is equivalent to above part number (should have same package)?

mmang.19
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Antoine Cros
Associate II

Hello,

Yes, whereas this is not explicitely stated in the datasheet, TS912 is unity gain stable.

Howevers, as most op-amps, stability depends on the load at the output. If a large capacitive load (>100pF) is used, stability has to be checked.

Best regards,

Antoine Cros

Op-Amps application team.