2021-08-23 4:23 PM
I need to run the TDA7293 because i wont to run 50 volts rails. I am so confused , i thought the parts were pin compatible. I have read the data sheet a few times and don't quite understand what is wrong. I am basically using the schematic of the TDA7294 but plugged into it a TDA7293.
Thanks
Scott
2021-08-26 12:41 AM
Should it be reminded that on TDA7293 pins 5, 11,12 are not N.C. and the connection of pin 6 can/should be different?
2021-08-26 7:06 AM
This is my schematic for the TDA7293, and i am running 50 volts on pins 7,8,13 and 15. Do you see anything wrong with this?
2021-08-26 7:08 AM