Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Resolved! TSC103 with no Vcc connected

I would like to use TSC103 in a system where the power line to be monitored is 48Vdc (63V maximum peak or steady state) and the ADC acquisition system is powered by a 5V voltage independent from the 48V line; so my doubt is if any failure can occur i...

Resolved! How to determine TS391 output voltage

In TS391 datasheet for max. Vol output voltage two values are specified:Under which conditions is 400mV resp. 700mV valid?NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support case...

0690X000006Dw0RQAS.png

LM2901 with one input outside the input common mode range

In the data sheet for TSX339 it says in chapter 6.1: "The output state is guaranteed as long as one input remains within the common modeinput voltage range (defined in the operating conditions table), and the other input remainsbetween -0.3 V and 16 ...

JSimo.19 by Associate II
  • 1540 Views
  • 6 replies
  • 0 kudos

How is make the mono setting about STA326?

Hello,I am using STA326 now and try to ​make mono setting.There is descrived the 1 Channel mono-parallel setting (addr: 0x05 value: 0xDF)but looks like output volume was lower than stereo.Is there another register setting?Let me know please.

HJM1 by Associate
  • 634 Views
  • 0 replies
  • 0 kudos

TDA7293 Bootstrap capacitor selection

I have built a circuit based on the tda7293 and it has burned instantly when connected.I have reviewed the layout but it has no errors.I am using Vs=36V and -Vs =-36V. The bootstrap capacitor is 22uFx50V. Is that capacitor well chosen?Do I have to us...

GDiaz by Associate
  • 945 Views
  • 0 replies
  • 0 kudos