Skip to main content
GDiaz
Visitor II
January 14, 2019
Question

TDA7293 Bootstrap capacitor selection

  • January 14, 2019
  • 0 replies
  • 763 views

I have built a circuit based on the tda7293 and it has burned instantly when connected.

I have reviewed the layout but it has no errors.

I am using Vs=36V and -Vs =-36V. The bootstrap capacitor is 22uFx50V.

Is that capacitor well chosen?

Do I have to use one with a working voltage greater than 2xVs?

Please clarify the working voltage of the capacitors in the manual.

This topic has been closed for replies.