Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Getting DAC output via I2S line

Hello, I want to send data to the DAC with the I2S protocol (assume we are sending an array) and see a sine wave at the output.At this point, I would like to ask: Does the DAC in the stm32f407vg model mean the CS43L22 IC or an internal DAC unit in it...

aozba.1 by Associate II
  • 1244 Views
  • 0 replies
  • 0 kudos

The TDA7492 is a dual BTL class-D audio amplifier with protection and diagnostic output. What are the thresholds for triggering the diffrent protections in particular open circuit

Im looking to find the threshold limit of Open Circuit protecion of an output channel, ive looked in all the datasheets but im sure it was around 1K ohm but i cant find a value anywhere. Does anyone know where i can get this data?ThanksJames

JHedg.1 by Associate II
  • 2331 Views
  • 8 replies
  • 0 kudos

TSH114 replacement

Need an operational amplifier for the video signal booster, with bandwidth >85MHz, able to work to a 75 Ohm line loads. I find the TSH114, but see the "obsolete" status. How name of the renewed one? Thank you.

Jendos by Associate
  • 747 Views
  • 0 replies
  • 0 kudos

Resolved! What is the dual supplie condition for TS393 comparator?

I have q question about TS393 comparator.Datasheet says : Wide single supply range 2.7 V to 16 V or dual supplies (±1.35 V to ±8 V)I dont understand dual supplies condition.What does mean "dual supplies (±1.35 V to ±8 V)"?

jsmit.1 by Associate
  • 954 Views
  • 1 replies
  • 0 kudos

We are looking to use the TS7221AILT comparator. It is rated for 10V, the absolute maximum is 12V. Our circuit uses 12V and we can't change the design at this time. What is the risk of using this device at the absolute maximum rating?

We are selecting this device as a substitute for our usual component. The output will only need to 'sink' 5.5 mA current. The 12V supply rail is well-regulated.

SHall.2 by Associate
  • 1095 Views
  • 1 replies
  • 0 kudos

Our customer would like to know whether the 7 items mentioned here are compliant with the Cobalt. There are some "undesirable" haloes on your general EMRT, and our customer mean, it can have a very negative effect on his business. Please check it.

Requested items are:49888R:     IC VN 800 PS-E                 SO 8 SMD ST                           VN800PSTR-E46602R:     Diode SMBJ 33 CA           DO 214AA SMD ST                           SMBJ33CA-TR46582R:     IC TS 321 AILT             SOT 23-...

IKreb.1 by Associate
  • 818 Views
  • 0 replies
  • 0 kudos