Hi Peter BENSCH,Thanks,Checked several times and it seems to be the issue of "lot of supply of these chips" (unbelievable, but its fact), as for the similar tests on the ICs (TL084CN) from the earlier batch of supply, I am getting better response up...
Hi Peter BENSCHFor a time being, let us consider only a voltage follower stage, where, the input is kept only at 1V rms (and also tried at 1V peak to peak) with the different frequencies, from 50Hz to 500kHz or so. The output, as expected is same as ...
Hi Peter BENSCHThanks for your response.As indicated earlier, the board using TL084C was designed for eight channel, with the attached schematic. Application is to use it for sinusoidal input signal of around 200kHz frequency with the gain up to 7 an...