7 Inch Display interface with STM32F746IGT custom development board issues?
Hai....,
I am using Waveshare STM32F746IGTx Development board and Waveshare 7 inch(1024x600) Capacitive Touch display QUADSPI (MT25QL128ABA1ESE-0SIT Micron Technology) own development board STMCube IDE and Custom External loader file.
After upload the program i am facing following error
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 4]
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 1]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:17.751
Verifying ...
Error: Data mismatch found at address 0x90000000 (byte = 0x99 instead of 0x00)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
where i am doing mistake, please give your suggestion.
Thanks & Regards
M. Govind