Skip to main content
PGroe.2
Associate III
March 29, 2021
Solved

STM32F469I-DISCO virtual com port USART3?

  • March 29, 2021
  • 1 reply
  • 1631 views

Hi there,

My new STM32F469I-DISCO just arrived I stumbled upon this part in user manual (UM1932):

4.11 Virtual COM port

The serial interface USART3 is directly available as a virtual COM port of the PC connected

to the ST-LINK/V2-1 USB connector CN1. The virtual COM port settings are configured as:

115200 b/s, 8 bits data, no parity, 1 stop bit, no flow control.

So I did a quick test in CubeIDE and enabled USART6 with default settings and just send one char to my USB-Serial Adapter to check on my PC if the char arrives... and it does.

Now I tried the same with USART3. As I plug in the DISCO board via its integrated STLink my Linux system tells me that a new serial device "ttyACM0: USB ACM" . So again I opened a serial terminal on ttyACM0 but no char gets received from the board.

What I am doing wrong? Or is my understanding wrong? Is "USART3" meant to be part of the STM32F103xxx STLInk or is it part of the boards STM32F469xxx?

This topic has been closed for replies.
Best answer by PGroe.2

Found a solution to myself:

When I enabled USART3 it enabled the default pins PD8 / PD9 but the lines that go from the STM32F469 to the STLink STM32F103 are PB10 / PB11 which are the alternate pins for USART3. So I enabled PB10 / PB11 as USART3 manually and violá, the char arrives at serial device ttyACM0.

1 reply

PGroe.2
PGroe.2AuthorBest answer
Associate III
March 29, 2021

Found a solution to myself:

When I enabled USART3 it enabled the default pins PD8 / PD9 but the lines that go from the STM32F469 to the STLink STM32F103 are PB10 / PB11 which are the alternate pins for USART3. So I enabled PB10 / PB11 as USART3 manually and violá, the char arrives at serial device ttyACM0.