cancel
Showing results for 
Search instead for 
Did you mean: 

Setting two CAN IDs in the Acceptance filter on STM32G474

SPang.1
Associate III

I am using the STM32G474E-EVAL1 board and the example FDCAN_Com_polling.

It is working and only accept ID of 0x111.

The code is:

  sFilterConfig.IdType = FDCAN_STANDARD_ID;
  sFilterConfig.FilterIndex = 0;
  sFilterConfig.FilterType = FDCAN_FILTER_MASK;
  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
  sFilterConfig.FilterID1 = 0x111;
  sFilterConfig.FilterID2 = 0x7FF;
  if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
  {
    Error_Handler();
  }

I now want the code to be able to accept two CAN IDs. Like 0x123 and 0x400.

I tried to set sFilterConfig.FilterID2 = 0x400 like this

  /* Configure reception filter to Rx FIFO 0 on both FDCAN instances */
  sFilterConfig.IdType = FDCAN_STANDARD_ID;
  sFilterConfig.FilterIndex = 0;
  sFilterConfig.FilterType = FDCAN_FILTER_MASK;
  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
  sFilterConfig.FilterID1 = 0x111;
  sFilterConfig.FilterID2 = 0x400;

but this won't accept 0x400.

I also tried to change  sFilterConfig.FilterIndex = 1;

  /* Configure reception filter to Rx FIFO 0 on both FDCAN instances */
  sFilterConfig.IdType = FDCAN_STANDARD_ID;
  sFilterConfig.FilterIndex = 1;
  sFilterConfig.FilterType = FDCAN_FILTER_MASK;
  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
  sFilterConfig.FilterID1 = 0x400;
  sFilterConfig.FilterID2 = 0x7FF;
  if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
  {
    Error_Handler();
  }

but that doesn't work either.

How can I set the filter to accept two CAN IDs ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
JEmi
Associate

I have the same problem with G4.