cancel
Showing results for 
Search instead for 
Did you mean: 

Chip Select for Quad SPI on STM32H7

RBharol
Associate III

Hi,

I am using Quad SPI on SHT32H7 and I am looking at examples in STMcube. My question is: Is Chip select for the QSPI handled by the port (inside the silicon) once set or is it my driver function that needs to do it like I had to in regular SPI drivers? I can't find any place in examples all over where Chip select is handled by user functions of even HAL drivers.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Bowman32
ST Employee

Hi @RBharol​ 

Do you mean where you can find the CS GPIO Pin configuration?

In the examples you can find it in msp file "stm32h7xx_hal_msp.c". Once the QUADSPI_CS GPIO pin configured, it is automatically managed by the QUADSPI.

Bouraoui

The NCS pin is managed by the QSPI peripheral, there are a limited number of choices, and the routing is controlled by the AF association in the GPIO configuration.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

STM32Cube_FW_H7_V1.5.0\Drivers\BSP\STM32H743I_EVAL\stm32h743i_eval_qspi.h

/* Definition for QSPI clock resources */
#define QSPI_CLK_ENABLE()              __HAL_RCC_QSPI_CLK_ENABLE()
#define QSPI_CLK_DISABLE()             __HAL_RCC_QSPI_CLK_DISABLE()
#define QSPI_CLK_GPIO_CLK_ENABLE()     __HAL_RCC_GPIOB_CLK_ENABLE()
#define QSPI_BK1_CS_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOG_CLK_ENABLE()
#define QSPI_BK1_D0_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D1_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D2_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK1_D3_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOF_CLK_ENABLE()
#define QSPI_BK2_CS_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOC_CLK_ENABLE()
#define QSPI_BK2_D0_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOH_CLK_ENABLE()
#define QSPI_BK2_D1_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOH_CLK_ENABLE()
#define QSPI_BK2_D2_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOG_CLK_ENABLE()
#define QSPI_BK2_D3_GPIO_CLK_ENABLE()  __HAL_RCC_GPIOG_CLK_ENABLE()
 
 
#define QSPI_FORCE_RESET()         __HAL_RCC_QSPI_FORCE_RESET()
#define QSPI_RELEASE_RESET()       __HAL_RCC_QSPI_RELEASE_RESET()
 
/* Definition for QSPI Pins */
#define QSPI_CLK_PIN               GPIO_PIN_2
#define QSPI_CLK_GPIO_PORT         GPIOB
/* Bank 1 */
#define QSPI_BK1_CS_PIN            GPIO_PIN_6
#define QSPI_BK1_CS_GPIO_PORT      GPIOG
#define QSPI_BK1_D0_PIN            GPIO_PIN_8
#define QSPI_BK1_D0_GPIO_PORT      GPIOF
#define QSPI_BK1_D1_PIN            GPIO_PIN_9
#define QSPI_BK1_D1_GPIO_PORT      GPIOF
#define QSPI_BK1_D2_PIN            GPIO_PIN_7
#define QSPI_BK1_D2_GPIO_PORT      GPIOF
#define QSPI_BK1_D3_PIN            GPIO_PIN_6
#define QSPI_BK1_D3_GPIO_PORT      GPIOF
 
/* Bank 2 */
#define QSPI_BK2_CS_PIN            GPIO_PIN_11
#define QSPI_BK2_CS_GPIO_PORT      GPIOC
#define QSPI_BK2_D0_PIN            GPIO_PIN_2
#define QSPI_BK2_D0_GPIO_PORT      GPIOH
#define QSPI_BK2_D1_PIN            GPIO_PIN_3
#define QSPI_BK2_D1_GPIO_PORT      GPIOH
#define QSPI_BK2_D2_PIN            GPIO_PIN_9
#define QSPI_BK2_D2_GPIO_PORT      GPIOG
#define QSPI_BK2_D3_PIN            GPIO_PIN_14
#define QSPI_BK2_D3_GPIO_PORT      GPIOG
/**
  * @brief QSPI MSP Initialization
  *        This function configures the hardware resources used in this example:
  *           - Peripheral's clock enable
  *           - Peripheral's GPIO Configuration
  *           - NVIC configuration for QSPI interrupt
  * @retval None
  */
__weak void BSP_QSPI_MspInit(QSPI_HandleTypeDef *hqspi, void *Params)
{
  GPIO_InitTypeDef gpio_init_structure;
 
  /*##-1- Enable peripherals and GPIO Clocks #################################*/
  /* Enable the QuadSPI memory interface clock */
  QSPI_CLK_ENABLE();
  /* Reset the QuadSPI memory interface */
  QSPI_FORCE_RESET();
  QSPI_RELEASE_RESET();
  /* Enable GPIO clocks */
  QSPI_CLK_GPIO_CLK_ENABLE();
  QSPI_BK1_CS_GPIO_CLK_ENABLE();
  QSPI_BK1_D0_GPIO_CLK_ENABLE();
  QSPI_BK1_D1_GPIO_CLK_ENABLE();
  QSPI_BK1_D2_GPIO_CLK_ENABLE();
  QSPI_BK1_D3_GPIO_CLK_ENABLE();
 
  QSPI_BK2_CS_GPIO_CLK_ENABLE();
  QSPI_BK2_D0_GPIO_CLK_ENABLE();
  QSPI_BK2_D1_GPIO_CLK_ENABLE();
  QSPI_BK2_D2_GPIO_CLK_ENABLE();
  QSPI_BK2_D3_GPIO_CLK_ENABLE();
 
  /*##-2- Configure peripheral GPIO ##########################################*/
  /* QSPI CLK GPIO pin configuration  */
  gpio_init_structure.Pin       = QSPI_CLK_PIN;
  gpio_init_structure.Mode      = GPIO_MODE_AF_PP;
  gpio_init_structure.Speed     = GPIO_SPEED_FREQ_VERY_HIGH;
  gpio_init_structure.Pull      = GPIO_NOPULL;
  gpio_init_structure.Alternate = GPIO_AF9_QUADSPI;
  HAL_GPIO_Init(QSPI_CLK_GPIO_PORT, &gpio_init_structure);
 
  /* QSPI CS GPIO pin configuration  */
  gpio_init_structure.Pin       = QSPI_BK1_CS_PIN;
  gpio_init_structure.Pull      = GPIO_PULLUP;
  gpio_init_structure.Alternate = GPIO_AF10_QUADSPI;
  HAL_GPIO_Init(QSPI_BK1_CS_GPIO_PORT, &gpio_init_structure);
 
  gpio_init_structure.Pin       = QSPI_BK2_CS_PIN;
  gpio_init_structure.Mode      = GPIO_MODE_AF_PP;
  gpio_init_structure.Pull      = GPIO_PULLUP;
  gpio_init_structure.Speed     = GPIO_SPEED_FREQ_VERY_HIGH;
  gpio_init_structure.Alternate = GPIO_AF9_QUADSPI;
  HAL_GPIO_Init(QSPI_BK2_CS_GPIO_PORT, &gpio_init_structure);
...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks, Bouraoui,

>> it is automatically managed by the QUADSPI.

That answers my question. Does it mean this limits the number of devices we can have on QSPI?

Thanks.

What do Bank 1 ann Bank 2 signify?

The H7 supports two QSPI devices. either as distinct devices, or paired to improve the bandwidth.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..