cancel
Showing results for 
Search instead for 
Did you mean: 

I am using a STM32G071. If I connect a STLINK to the uC, and then I disconnect it, also after a reset cycle, BOOT0 pin status is ignored and the boot happens always on Flash Memory instead of System Memory. Why? Is it normal?

ATPG
Associate II

I want to use BOOT0 pin to select System Memory boot.

nBOOT0 = 0, nBOOT1 = 1, nBOOT_SEL = 0 bits in user config are well programmed.

Boot works well if my uC is coming from a POR or power cycle. But if I connect a ST-LINK to the uC and simply open the STM32CubeProgrammer application, and then I disconnect the programmer, also after a nRST hole the BOOT0 pin status is ignored and I cannot reach the system memory from boot anymore.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

Did you check the option bits? BOOT0 can made to be ignored.

ATPG
Associate II

Hi,

With STM32CubeProgrammer tihs is my option bits configuration.

0693W000007ZD9TQAW.pngI applied and then I read it back to check, and they re right.

nBOOL_SEL to 0 should guarantee the boot selection with boot0 pin.

The strange tihng is that happen just if I've connected the programmer before. If I power off and power on my board it works perfectly.