Skip to main content
MSori.1
Associate
February 24, 2021
Solved

VCC on ST-Link devices to power the target board

I have one ST-Link/V2 and one ST-Link/V2 ISOL and I experience following difference which I did not expect:

  • ST-Link/V2 provides 3.3V to power the target's µC on PIN 1 of the flat ribbon cable
  • ST-Link/V2 ISOL does NOT provide 3.3V on that pin with the same configuration used in ST-Link utility

Is this by design, that intentionally the ISOL variant does not provide the 3.3V output or is there anyhow the possibility to recofigure the device to also provide the target power?

This topic has been closed for replies.
MSori.1
MSori.1Best answer
Associate
February 24, 2021

@Community member​: Okay solved. I mixed it up with PIN 19, which really provides 3.3V on non-ISOL only according to ST-Link User Manual.

3 replies

Tesla DeLorean
Guru
February 24, 2021

>>ST-Link/V2 provides 3.3V to power the target's µC on PIN 1 of the flat ribbon cable

No, in the authentic devices it expects YOUR TARGET to provide a voltage that the ST-LINK target side drivers/buffers should use as an IO level to communicate with the target.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MSori.1
MSori.1Author
Associate
February 24, 2021

With "authentic" you mean "originally from ST"? I have one original from ST and I definitely can measure this voltage level at that pin. And it does not look like that someone from our own team have opened it in the past to implement this voltage supply.

MSori.1
MSori.1AuthorBest answer
Associate
February 24, 2021

@Community member​: Okay solved. I mixed it up with PIN 19, which really provides 3.3V on non-ISOL only according to ST-Link User Manual.