cancel
Showing results for 
Search instead for 
Did you mean: 

Hi. Can anyone tell me how to BlueNRG-X_Flasher_GUI.exe to program the target chip? Command Line Download Fireware......

TYang.5
Associate

Dear ALL,

I can use BlueNRG-X_Flasher_GUI.exe to program the target chip,please see attached picture 1

0693W000007CyF3QAK.png 

But I want to use BlueNRG-X_Flasher_Launcher.exe to download, but I can’t do it. Here

is my attempt to follow the Commands.

Below is the command I tried:

C:\Users\TenoYang>BlueNRG-X_Flasher_Launcher.exe flash -SWD -all -f "C:\STLink.b

in"

Working on ST LINK:

 1)\ (x)

09:15:16.542:

STLink A -> Waiting device to flash...09:15:16.598:

STLink A -> Waiting device to flash...09:15:16.653:

STLink A -> Waiting device to flash...09:15:16.743:

STLink A -> Waiting device to flash...09:15:16.795:

STLink A -> Waiting device to flash...09:15:16.846:

STLink A -> Waiting device to flash...09:15:16.897:

STLink A -> Waiting device to flash...09:15:16.947:

STLink A -> Waiting device to flash...09:15:16.996:

STLink A -> Waiting device to flash...09:15:17.052:

STLink A -> Waiting device to flash...09:15:17.098:

STLink A -> Device to flash not connected.

****

INPUT PARAMETERS FOR FLASH OPERATION****

-

OPERATING MODE = SWD

-

CMSISDAP = DISABLE

-

FREQUENCY = 4000

-

BLUENRG-1 DEVICE FILE = C:\STLink.bin

-

BLUENRG-2 DEVICE FILE = C:\STLink.bin

-

BLUENRG-LP DEVICE FILE = C:\STLink.bin

- VERIFY

= False

- MASS

ERASE = False

- START

ADDRESS = 0x10040000 (only for .bin image file)

- READOUT

PROTECTION = False

- MAC

ADDRESS OPTION = False

- LOG =

False

****

RESULTS OF FLASH OPERATION ***

1 -

Device connected with STLink A (\x34\x3f\x6c\x06\x41\x55\x30\x39\x43\x16\x21

\x57)

Device =

None

Command

-> FLASH = Fail

WARNING

MESSAGE:

Device to

flash not connected.

Q:How to use BlueNRG-X_Flasher_Launcher.exe to download a bin file to the target chip

(BlueNRG-LP QFN48)???

Why doesit prompt that the device cannot be connected? Is my commands not correct?

could you give me some advice.

Looking forward to your reply, thank you very much!!

0 REPLIES 0