cancel
Showing results for 
Search instead for 
Did you mean: 

adding Path Variable to the project isn't working

MFawzy
Associate II

I Added a path variable to the project

and when i'm using this variable with the include files, it can't be recognized

so what is problem?

3 REPLIES 3
MFawzy
Associate II

it seems that the images aren't attached to my post0693W000007CG3NQAW.png0693W000007CG38QAG.png

Pavel A.
Evangelist III

Unfortunately Path variables cannot be used in CDT settings (Paths and symbols, etc). For this you should define a Build variable (under C++ Build).

At least in this version of Eclipse CDT.

Path variables only work in definition of linked resources.

Yes, very annoying and silly :(

--pa

unbelievable, I'm using this feature with code composer from TI which is based on eclipse from about 7 years ago and this feature was supported.

Thank you very much for your answer!

Mohammed