Skip to main content
Parmin Nayani
Associate III
November 7, 2020
Solved

How to create ZigBee project for stm32wb55 using cubemx? IDE is CubeIDE.

  • November 7, 2020
  • 8 replies
  • 1915 views

I would like to create a ZigBee application on STM32WB55 controller for CubeIDE. Unfortunately there are no .IOC example files for ZigBee. What components do I need to select in CubeMX to be able to use ZigBee? Should I enable BLE or THREAD (WPAN). In my sample project though I enabled RTC, under RTC/LCD source mux in clock configuration "enable css" is disabled so not able select LSE. What is the mistake I made. Thank you for your time.

This topic has been closed for replies.
Best answer by Houssem CHAABANI

Dear @Parmin Nayani​ 

In order to enable zigbee in STM32CubeMX, you need to activate:

  • RF
  • RTC
  • HSEM

You can find RF under connectivity, RTC under timers and HSEM under system core.

After that you activate ZIGBEE under Middleware -> STM32_WPAN.

Best regards,

Houssem

8 replies

Houssem CHAABANI
Houssem CHAABANIBest answer
Visitor II
November 9, 2020

Dear @Parmin Nayani​ 

In order to enable zigbee in STM32CubeMX, you need to activate:

  • RF
  • RTC
  • HSEM

You can find RF under connectivity, RTC under timers and HSEM under system core.

After that you activate ZIGBEE under Middleware -> STM32_WPAN.

Best regards,

Houssem

Parmin Nayani
Associate III
November 9, 2020

Hello Houssem CHAABANI,

Thank you very much for the reply. So There is no need to enable/select either BLE or MESH options?

Best regards

NPS

Houssem CHAABANI
Visitor II
November 9, 2020

Dear @Parmin Nayani​ ,

Yes if you only need ZIGBEE you don't need to activate anything else.

Kind regards,

Houssem