cancel
Showing results for 
Search instead for 
Did you mean: 

SPC58EC DISP not build aplications

RPari.1
Associate II

I'm loading aplication's SPC58EC DISP, and debugging, but if I change the main.c this is the 9 problens. What it's, please?

Another problem is that if I change and build the project, the changes not appear

in the UDESTARTERKIT.

5 REPLIES 5
Erwan YVIN
ST Employee

Hello ,

All the applications based SPC58EC DISP are built, flashed and tested on our continuous integration.

Could you detailed your problem ?

Best regards

Erwan

RPari.1
Associate II

I only had created one variable in main.c

If i change anyfing in main.c have 9 problens.

We see that the project folder is only read.

If I uncheck box read only in the folder , after building it's return to read only.

Erwan YVIN
ST Employee

Hello ,

The problem can come from CDT. (C/C++ Development Tooling) Symbol Issues on the compiler.

could you send me the screenshot ?

could you detail your issue and show the errors logs ?

Best regards

Erwan

0693W000004JfwtQAC.png0693W000004JfwjQAC.pngHello,

below it's 9 problens,

 If I change the main.c and build the sisten not such the directory,

I see again if only write in the main one variable for example:

the SPC5studio don't creat the code.

Hello ,

Ok , i see your error logs 😉

Have you clicked on generate before compilation ?

could you export and send me your application if there is no confidential code?

What is your installation details ?

Best regards

Erwan