cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to start General Discovery Mode along with general discoverable mode in BlueNRG-2

Bilal1
Associate

I want to discover the peripheral devices with BlueNRG-2 central role.The initializing function set up the public address with ac_write_config_data and than initialize the Gatt layer with aci_gatt_init function. Finally I call gap_init with the following parameters: (GAP_CENTRAL_ROLE|GAP_PERIPHERAL_ROLE (0x04|0x01), PRIVACY_DISABLED (0x00) and device name characteristic length: 0x07. All aci functions returns BLE_STATUS_SUCCESS (indicating the initialization was successful) but as soon as I start general discovery procedure with aci_start_general_discovery_proc it always returns (0x82) error.

Can anybody suggest a solution to this problem?

Regards,

0 REPLIES 0