cancel
Showing results for 
Search instead for 
Did you mean: 

Which FlexCAN modules are available in 3-CAN SPC582B?

Yannek
Associate III

Although SPC582B family has up to 7 FlexCAN modules, some units have only 3 (i.e. SPC582B60E1CD00X).

Which 3 of 7 CAN modules are available in this processor?

Since SPC5Studio shows 7 CANbuses for this processor, I don't know which I/O should I design for CANbuses.

1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

This information will be published in DS rev4

View solution in original post

6 REPLIES 6
Erwan YVIN
ST Employee

Yes , in SPC5Studio , we are seeing 7 Can Buses

You can use the Pinmap Wizard in order to determine which I/O Buses are designed for CAN Bus

It is very useful.

I am checking in the RM.

and check with experts

Best regards

Erwan

0690X00000D8TrHQAV.png

Yannek
Associate III

Unfortunately, in this case, I cannot use SPC5Studio to see which I/O pins are designed for CANbus in SPC582B60E1CD00X.

SPC5Studio shows that this processor has 7 CANbuses, while actually it has only 3.

In SPC5Studio there is no choice between SPC582B60E1CD00X (3 CANbuses) and SPC582B60E1MH00Y (7 CANbuses):

0690X00000D8UnfQAF.png

Waiting for the answer from experts 🙂

Yannek

JoniS
Senior

I bet you get the information faster from datasheet of the given mcu.​

I bet you don't, JoniS. Not only faster. Not at all.

Yannek
Associate III

Hi Erwan,

Would you have any information in this topic, please?

Our project stucked, because we don't know which pins should be used...

Best,

Yannek

Giuseppe DI-GIORE
ST Employee

This information will be published in DS rev4