Skip to main content
aziubin
Graduate
March 16, 2024
Solved

Teseo-LIV3FL vs. Teseo-LIV3F

  • March 16, 2024
  • 2 replies
  • 2507 views

Hello!

Can you please help with the differences between Teseo-LIV3FL and Teseo-LIV3F modules, does LIV3FL have all the features of LIV3F plus low power, are there any reasons why to prefer LIV3F over LIV3FL nowadays, or it is recommended to always use LIV3FL instead of LIV3F for new design?

Thanks.

 

This topic has been closed for replies.
Best answer by Peter BENSCH

TESEO-LIV3FL not only has a built-in SMPS and requires less energy than TESEO-LIV3F, but also operates at a lower minimum voltage.

Above all, both are on the 7-year Product Longevity List, but TESEO-LIV3FL will be available for almost 2 years longer:

Hope it answers your question?

Good luck!
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
March 18, 2024

TESEO-LIV3FL not only has a built-in SMPS and requires less energy than TESEO-LIV3F, but also operates at a lower minimum voltage.

Above all, both are on the 7-year Product Longevity List, but TESEO-LIV3FL will be available for almost 2 years longer:

Hope it answers your question?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
April 4, 2024

In addition to the comments above

Teseo LIV3FL has an operating range of 1.8V to 3.3V.

Teseo LIV3FL also supports timing.

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.