cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt behavior of LSM6DSOX?

TSchi.2269
Associate III

I am looking to create a project where I can set/latch the interrupt pin INT1 on high when the LSM6DSOX is detecting state X (where X is state 1/2/3 etc.) and goes down (low) when in a generic/static state (state 0). How is this possible? I found in one of the application notes that the PAGE_RW flag (17h) has something to do with the flag. However, I am not able to find how I can customize the output signal like described above.

Has anyone experience with interrupts and how should one do this?

1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @TSchi.2269​ , is this topic related to this thread? Regards

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @TSchi.2269​ , is this topic related to this thread? Regards