Skip to main content
Gowtham shanmugaraj
Associate
September 7, 2019
Question

I have trouble getting ETM instruction trace out of stm32f411ve.

  • September 7, 2019
  • 4 replies
  • 2013 views

I've configured GPIO for trace , enabled trace in MCUDEBUG and coredebug registers and enabled ETM and started it.when I view the trace pins in a ​logic analyser.. there seems to be no activity on the trace pins. If you have example code for ETM trace using Stm32F4 please provide that.

​

Thanks in advance​

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
September 7, 2019

Keil had projects and debug configuration files for it ULINKPro and MCBSTM32F400

 _WDWORD(0x40023830, _RDWORD(0x40023830) | 0x00000010); // RCC_AHB1ENR: IO port E clock enable
 _WDWORD(0x40021000, 0x00002AA0); // GPIOE_MODER: PE2..PE6 = Alternate function mode
 _WDWORD(0x40021008, 0x00003FF0); // GPIOE_OSPEEDR: PE2..PE6 = 100 MHz speed
 _WDWORD(0x4002100C, 0x00000000); // GPIOE_PUPDR: PE2..PE6 = No Pull-up/Pull-down
 _WDWORD(0x40021020, 0x00000000); // GPIOE_AFRL: PE2..PE6 = AF0
 _WDWORD(0xE0042004, 0x000000E7); // DBGMCU_CR Enable 4-bit Trace

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gowtham shanmugaraj
Associate
September 7, 2019

i don't want to use ULINKPRO. I just want to capture the trace pins in a logic analyser. How can I do that? Below is the code i execute after configuring gpio. But i observe no activity on trace pins. What do you think is the problem here?

 DBGMCU->CR |= DBGMCU_CR_TRACE_IOEN; /* enable trace io */
 DBGMCU->CR |= (3u<<DBGMCU_CR_TRACE_MODE_Pos); /* enable 4 pin data + 1 pin clock */
 
 CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk; /* enable TPIU */
 
 ETF_BASE_PTR->FCR |= 3u; 
 
 ETM_BASE_PTR->LAR = 0xC5ACCE55; /* unlock ETM registers */
 ETM_BASE_PTR->CR = 0x00001D1Eu;
 while(!((ETM_BASE_PTR->SR) & (1u<<1u))); 
 ETM_BASE_PTR->TRIGGER = 0x0000006Fu;
 ETM_BASE_PTR->EEVR = 0x0000006Fu; 
 ETM_BASE_PTR->TECR1 = 0x00000001u; 
 ETM_BASE_PTR->CR = 0x0000191Eu; 
 while(((ETM_BASE_PTR->SR) & (1u<<1u)));

Tesla DeLorean
Guru
September 7, 2019

It was cited as a working example that could be reviewed and probed.

​ARM might have a document for debugger writers. Segger might scripts.

I'll query one of my contacts.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gowtham shanmugaraj
Associate
September 7, 2019

In the debug configuration file, that keil provides for u link pro, which you mentioned, they do only GPIO configuration... I guess Trace / ETM configuration​ is done by the IDE itself via JTAG if trace is enabled? or you pasted only a part of the script?. It would be really helpful if you can provide some insights..