cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 if do not use DLE, then SHCI_C2_BLE_Init return error

Vyacheslav
Senior II

STM32WB55 if do not use DLE, then SHCI_C2_BLE_Init return error

Hi !

If in structure SHCI_C2_Ble_Init_Cmd_Packet_t

set ExtendedPacketLengthEnable = 0 (disable DLE),

then result of calling SHCI_C2_BLE_Init()

is error = 72.

This error not in SHCI_CmdStatus_t enum and don`t found in any documents.

Question: where to find example ho to use stack without DLE ?

Second (comment):

Event "HCI_LE_DATA_LENGTH_CHANGE_EVENT" (AN5270) located in "HCI LE META events", but he is not in list of events in "hci_const.h" that's why I have to write like this:

case 0x07: //HCI_LE_DATA_LENGTH_CHANGE_EVENT

{

...

}

0 REPLIES 0