cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560 - eMIOS

ssk
Associate II
Posted on August 20, 2015 at 18:04

Hello,

I am using eMIOS module for SPC560D40L3 MCU for generating PWM. I am using default configuration for the SPCStudio project with no change to FMPLL0 and Clocks settings. My target uses 8MHz external XTAL. With this, I am trying to generate a PWM for frequency ranging from 15Hz to 600Hz. I observed that the PWM channel is not giving exact frequency PWM on the output. The difference is small at lower values but goes on increasing as the frequency rises (@ 125Hz at 600Hz). Why is this behavior for eMIOS module? Is any additional configuration required?

Thanks in advance.

Mike.
3 REPLIES 3
Erwan YVIN
ST Employee
Posted on August 24, 2015 at 11:29

Hello mike ,

I am checking the issue with the EMIOS experts.

      Best regards

                 Erwan

ssk
Associate II
Posted on August 25, 2015 at 16:03

Hello Erwan,

Any updates on this? Your earliest help will be highly appreciated.

Thanks.

Mike.

Erwan YVIN
ST Employee
Posted on August 25, 2015 at 17:58

Dear Mike ,

i have sent an email concerning this issue.

            Best Regards

                         Erwan