cancel
Showing results for 
Search instead for 
Did you mean: 

need help for CAN Configuration !

nr_naik
Associate II
Posted on November 07, 2008 at 07:18

need help for CAN Configuration !

1 REPLY 1
nr_naik
Associate II
Posted on May 17, 2011 at 09:56

I want to run the CAN @ 1Mbps for PCLK of 48MHz. Need help for settings of the can bit rate settings.

I tried 1Mbps @8MHz Pclk ( which is available in the CAN library function ) , that works fine.

Now using the calculation information the settings for 1Mbps with 48MHz PCLK , comes out to be Time QUANTA = 8, Tseg1 = 4, Tseg2 = 3, BRP = 6 & SJW = 1 to 4. But this setting does not work.

NEED Help for this settings.

Need these settings and guidance for calculations.