Posted on May 17, 2011 at 12:58is there any limitation or hurdle or bottle necks in using the internal crystal oscillator on STM32F103RB. This is a 64 pin TQFP package. Also, if internal oscillator suffices the need of micro.. can i use the OSC-in a...
Posted on May 17, 2011 at 11:32Hello, I want to use Ethernet port availabe on STr9 and interface my system using TCP / IP protocol. I searched for the ready code availabe on ST9 application notes , but i could not get implementation for TCP protoco...
Posted on May 17, 2011 at 09:56I want to run the CAN @ 1Mbps for PCLK of 48MHz. Need help for settings of the can bit rate settings. I tried 1Mbps @8MHz Pclk ( which is available in the CAN library function ) , that works fine. Now using the calcula...
Posted on May 17, 2011 at 09:56Hello, I want to use Ethernet port availabe on STr9 and interface my system using TCP / IP protocol. I searched for the ready code availabe on ST9 application notes , but i could not get implementation for TCP protocol...