cancel
Showing results for 
Search instead for 
Did you mean: 

test on Mifare Classic with CR95HF

elasa
Associate
Posted on September 16, 2016 at 13:44

Hello,

I'm trying to communicate with a Mifare classic card but I can't.

I'm following the example described on the datasheet (page 60) and when it comes to auth, I'm sending the command:

0x04 0x09 0x60 0x00 0x04 0x00 0xd1 0x00 0x3d 0x00 0x18

But the answer is alway the same: 0x87 0x00

I've tried modifying the frame waiting values, but the error persists.

Any idea?

Thanks in advance!

#cr95hf-st95hf
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on September 26, 2016 at 12:04

Hello ELasa,

As mention in the datatsheet :

MIFARE and MIFARE

®

 Classic are trademark of NXP B.V. and are used under license.

CR95HF is able to manage the Parity Framing mode compatible with MIFARE

®

 classic requirements. However, access to Authenticated state must be support by an external secure host which embeds the MIFARE

®

  Classic library. So you have to check with the TAG provider specifications in order to manage the entire sequence and protocol which is not natively done by the CR95HF.  

Regards

View solution in original post

1 REPLY 1
Posted on September 26, 2016 at 12:04

Hello ELasa,

As mention in the datatsheet :

MIFARE and MIFARE

®

 Classic are trademark of NXP B.V. and are used under license.

CR95HF is able to manage the Parity Framing mode compatible with MIFARE

®

 classic requirements. However, access to Authenticated state must be support by an external secure host which embeds the MIFARE

®

  Classic library. So you have to check with the TAG provider specifications in order to manage the entire sequence and protocol which is not natively done by the CR95HF.  

Regards