cancel
Showing results for 
Search instead for 
Did you mean: 

NETMF bugs with STM32F429IDiscovery

rocketbob
Associate
Posted on March 19, 2014 at 23:03

Hello,

I've noticed that the .NET micro framework port provided by ST for the STM32F429IDiscovery board has a bug with LCD code.   If one tries to use the .flush method on a bitmap object while specifying X,Y, Width, Height parameters those parameters incorrectly compute the area the bitmap should be flushed.

Also there are no methods provided to change the orientation of the LCD.  How would I go about getting the modified porting kit changes made by ST so I could add this functionality myself?

Thanks,

Bob

#netmf-lcd-429-bitmap-flush
1 REPLY 1
Just Matt
Associate III
Posted on March 20, 2014 at 17:16

I cant answer your question sadly...

However, if ST would release the source for this, so we can make changes like this ourselves.

ST...common?