cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 Flash tool

mahendrai
Associate II
Posted on November 17, 2014 at 15:45

How to flash STM32F429 LQFP176 through USART during production? I have tried STM32 Flash Loader demonstration tool but it looks like STM32F429 with 2MB flash is not supported. Any other tool to flash this chip during mass production?

TIA

MR 
1 REPLY 1
Posted on November 17, 2014 at 16:40

The underlying protocol is pretty simple, and source code for the Flash Loader Demonstrator is provided. There are also Open Source solutions. A coder with Windows/Linux experience should be able to build a solution in a couple of man days or less.

The loader could also push in code to RAM, and then use a more robust XMODEM/YMODEM transfer to complete the job if you're more familiar with those protocols. See also ST's IAP examples.

What's your budget for a commercial solutions, per station?

Segger has a number of JTAG/SWD based solutions. With USB there's DFU Manager.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..