cancel
Showing results for 
Search instead for 
Did you mean: 

STC3115 Questions

jason239955_st
Associate III
Posted on July 26, 2016 at 10:33

Hi Sir/Mdm,

I have few questions regarding STC3115. After implementation, I have noticed that voltage & current measurements are working properly, however the SOC value is never updated. 

1. Is it normal? 

2. Does the STC3115 need to go through a minimum number of charge/discharge cycles before it can update the SOC value? 

3. Is there any triggering events to start updating the SOC value? 

Regard's

Jason

#l6699a-battery-charger-d #stc3115-issue-startup
1 REPLY 1
Gregory Go.
Senior II
Posted on September 24, 2016 at 10:59

Hello,

Please see answers below:

1. Is it normal? 

No, this is not the normal behavior. 

The SOC is the most important expected information from a fuel gauge.

2. Does the STC3115 need to go through a minimum number of charge/discharge cycles before it can update the SOC value? 

No, the first SOC is available after 2s.

3. Is there any triggering events to start updating the SOC value? 

No. But this issue usually arise when the gas gauge is not running properly. 

It could be because the pin BATD is floating, avoiding the gas gauge to start the battery monitoring.

Once the hardware issue is resolved, it is then recommended to use ST open source driver to initialize properly the device and run it.

You can find a FAQ of common STC3115 questions/issue from the community here:

https://github.com/st-sw/STC3115GenericDriver/wiki/STC3115-FAQ

It is similar for STC3117.

Regards