cancel
Showing results for 
Search instead for 
Did you mean: 

CODE FOR RX AND TX BUFFER

adeemkazi92
Associate II
Posted on September 30, 2015 at 15:21

CAN SOMEONE PROVIDE ME WITH FULL WORKING CODE OF RX AND TX BUFFER FOR RECEIVING AND TRANSMITTING DATA IN STM32F07 USART.

ANY HELP IS WELCOME.THANKS IN ADVANCE
2 REPLIES 2
jpeacock
Associate III
Posted on September 30, 2015 at 21:10

Show us what you have completed so far and where you are getting errors.

If you are only looking for a programmer to write code for you then your best option is to run a help want ad on a local website or newspaper, stating the skills you need to hire and what pay rate you will offer.

Have you looked at the ST code examples?

  Jack Peacock

Amel NASRI
ST Employee
Posted on October 01, 2015 at 10:15

Hi kazi.adeem,

I agree with Jack's point of view.

Any way, I suggest you take examples available in

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260612

as a start point to develop your own application.

You may find examples in this folder after downloading the package: STM32Cube_FW_F0_V1.4.0\Projects\STM32F070RB-Nucleo\Examples\UART.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.