2008-02-24 08:28 PM
temp LM75 got strange value
#stm32-lm75-wrong-temp-value #lm75-stm32f103x-temp-register-s2011-05-17 03:24 AM
Hello!
I got a problem with the LM75 tempsensor that are on the stm32 eval board. When I read the temp value I got the result to 207 and that is 0xCF. Seems a bit high something like 75 celcius degress. And to get any value from it I need to read 2 times and the second time then I got results from it. What can be wrong?2011-05-17 03:24 AM
your adc is not configured correctly,
I think you have dual mode or injected channels ? or DMA increase enabled ? what board is it you talk about ? quite alot of STM32 boards exist :-)2015-05-26 05:01 AM
stm32f103ze.. muc eval board....... i m getting temprature value as 74 degree..
just using muc and stlm75 temprature sensor... what is problem i can find out as i m new in embedded field.. plz help.. code file attached.. my code is below..... #include ''stm32f10x.h'' #include ''stdio.h'' #define LM75_ADDR 0x90 void usart_send_char(unsigned char data) { while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, data); } void SENDU(char *string) { while(*string!='\0') { usart_send_char(*string); string++; } } void init_usart1(void) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; /* Enalbe clock for USART1, AFIO */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1,ENABLE); /***** tx and rx pin 9 and 10 of gpioa*****/ /* GPIOA PIN9 alternative function Tx */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* GPIOA PIN9 alternative function Rx */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); /* usart initilize*/ USART_DeInit(USART1); USART_Cmd(USART1,ENABLE); USART_InitStructure.USART_BaudRate =9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_Mode = USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; /* Configure USART1 */ USART_Init(USART1, &USART_InitStructure); } uint8_t LM75_Init() { GPIO_InitTypeDef PORT; I2C_InitTypeDef I2CInit; /* Enable GPIO & I2C clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOB,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); // GPIO_PinRemapConfig(GPIO_Remap_I2C1, ENABLE); /* Configure I2C pins: SCL and SDA */ PORT.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; PORT.GPIO_Mode = GPIO_Mode_AF_OD; PORT.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOB,&PORT); /* Configure PB.5 as Input pull-up, used as TemperatureSensor_INT */ PORT.GPIO_Pin = GPIO_Pin_5; PORT.GPIO_Speed = GPIO_Speed_10MHz; PORT.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOB, &PORT); /* I2C configuration */ I2C_DeInit(I2C1); // I2C reset to initial state I2CInit.I2C_Mode = I2C_Mode_I2C; // I2C mode is I2C I2CInit.I2C_DutyCycle = I2C_DutyCycle_2; // I2C fast mode duty cycle I2CInit.I2C_OwnAddress1 = 0x00; // This device address (7-bit or 10-bit) I2CInit.I2C_Ack = I2C_Ack_Enable; // Acknowledgment enable I2CInit.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; // choose 7-bit address for acknowledgment I2CInit.I2C_ClockSpeed = 200000; I2C_Cmd(I2C1,ENABLE); // Enable I2C I2C_Init(I2C1,&I2CInit); // Configure I2C while (I2C_GetFlagStatus(I2C1,I2C_FLAG_BUSY)); // Wait until I2C free return 0; } // Read 16-bit LM75 register uint16_t LM75_ReadReg() { uint16_t value; // char str5[]=''abc.\n''; //char str6[]=''def.\n''; /*transmission--------------------------------------------------------------------*/ I2C_GenerateSTART(I2C1,ENABLE); while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_MODE_SELECT)); // Wait for EV5 I2C_Send7bitAddress(I2C1,LM75_ADDR,I2C_Direction_Transmitter); // Send slave address //SENDU(str5); while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); // Wait for EV6 //SENDU(str6); I2C_SendData(I2C1,0x00); // Send register address while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // Wait for EV8 /*-----------------reception-----------------------------------------------------------------*/ I2C_GenerateSTART(I2C1,ENABLE); // Send repeated START condition (aka Re-START) while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_MODE_SELECT)); // Wait for EV5 I2C_Send7bitAddress(I2C1,LM75_ADDR,I2C_Direction_Receiver); // Send slave address for READ while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); // Wait for EV6 while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave) value = (uint16_t)I2C_ReceiveData(I2C1)<<8 ; // Receive high byte I2C_AcknowledgeConfig(I2C1,ENABLE); // enableI2C acknowledgment while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave) value |= I2C_ReceiveData(I2C1); // Receive low byte I2C_AcknowledgeConfig(I2C1,DISABLE); // Disable I2C acknowledgment I2C_GenerateSTOP(I2C1,ENABLE); // Send STOP condition return value; } int main(void) { uint16_t temp; //char str1[]=''\nSTM32F103ZET6 is online.\n''; //char str2[]=''ready.\n''; //char str3[]=''lm75 init fail.\n''; //char str9[]=''out of reg conf .\n''; char str4[]=''temp val is.hex..\n''; char st[20]; SystemInit(); init_usart1(); //SENDU(str1); if (!LM75_Init()) { //SENDU(str2); } else { // SENDU(str3); while(1); } SENDU(str4); temp = LM75_ReadReg()>>7; //Temprature register address 0x00 sprintf(st,''temp=%d'',temp); SENDU(st); while(1); } ________________ Attachments : lm75_i2c.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0dV&d=%2Fa%2F0X0000000bbw%2FnuoCDsW6hI_FUkKFw3I7eIAPPxONCYtVrBd0vLWZl8Y&asPdf=false2015-05-26 05:03 AM
stm32f103ze.. muc eval board....... i m getting temprature value as 74 degree..
just using muc and stlm75 temprature sensor... what is problem i can find out as i m new in embedded field.. plz help.. code file attached.. my code is below..... #include ''stm32f10x.h'' #include ''stdio.h'' #define LM75_ADDR 0x90 void usart_send_char(unsigned char data) { while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, data); } void SENDU(char *string) { while(*string!='\0') { usart_send_char(*string); string++; } } void init_usart1(void) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; /* Enalbe clock for USART1, AFIO */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1,ENABLE); /***** tx and rx pin 9 and 10 of gpioa*****/ /* GPIOA PIN9 alternative function Tx */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* GPIOA PIN9 alternative function Rx */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); /* usart initilize*/ USART_DeInit(USART1); USART_Cmd(USART1,ENABLE); USART_InitStructure.USART_BaudRate =9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_Mode = USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; /* Configure USART1 */ USART_Init(USART1, &USART_InitStructure); } uint8_t LM75_Init() { GPIO_InitTypeDef PORT; I2C_InitTypeDef I2CInit; /* Enable GPIO & I2C clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOB,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); // GPIO_PinRemapConfig(GPIO_Remap_I2C1, ENABLE); /* Configure I2C pins: SCL and SDA */ PORT.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; PORT.GPIO_Mode = GPIO_Mode_AF_OD; PORT.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOB,&PORT); /* Configure PB.5 as Input pull-up, used as TemperatureSensor_INT */ PORT.GPIO_Pin = GPIO_Pin_5; PORT.GPIO_Speed = GPIO_Speed_10MHz; PORT.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOB, &PORT); /* I2C configuration */ I2C_DeInit(I2C1); // I2C reset to initial state I2CInit.I2C_Mode = I2C_Mode_I2C; // I2C mode is I2C I2CInit.I2C_DutyCycle = I2C_DutyCycle_2; // I2C fast mode duty cycle I2CInit.I2C_OwnAddress1 = 0x00; // This device address (7-bit or 10-bit) I2CInit.I2C_Ack = I2C_Ack_Enable; // Acknowledgment enable I2CInit.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; // choose 7-bit address for acknowledgment I2CInit.I2C_ClockSpeed = 200000; I2C_Cmd(I2C1,ENABLE); // Enable I2C I2C_Init(I2C1,&I2CInit); // Configure I2C while (I2C_GetFlagStatus(I2C1,I2C_FLAG_BUSY)); // Wait until I2C free return 0; } // Read 16-bit LM75 register uint16_t LM75_ReadReg() { uint16_t value; // char str5[]=''abc.\n''; //char str6[]=''def.\n''; /*transmission--------------------------------------------------------------------*/ I2C_GenerateSTART(I2C1,ENABLE); while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_MODE_SELECT)); // Wait for EV5 I2C_Send7bitAddress(I2C1,LM75_ADDR,I2C_Direction_Transmitter); // Send slave address //SENDU(str5); while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); // Wait for EV6 //SENDU(str6); I2C_SendData(I2C1,0x00); // Send register address while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // Wait for EV8 /*-----------------reception-----------------------------------------------------------------*/ I2C_GenerateSTART(I2C1,ENABLE); // Send repeated START condition (aka Re-START) while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_MODE_SELECT)); // Wait for EV5 I2C_Send7bitAddress(I2C1,LM75_ADDR,I2C_Direction_Receiver); // Send slave address for READ while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); // Wait for EV6 while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave) value = (uint16_t)I2C_ReceiveData(I2C1)<<8 ; // Receive high byte I2C_AcknowledgeConfig(I2C1,ENABLE); // enableI2C acknowledgment while (!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave) value |= I2C_ReceiveData(I2C1); // Receive low byte I2C_AcknowledgeConfig(I2C1,DISABLE); // Disable I2C acknowledgment I2C_GenerateSTOP(I2C1,ENABLE); // Send STOP condition return value; } int main(void) { uint16_t temp; //char str1[]=''\nSTM32F103ZET6 is online.\n''; //char str2[]=''ready.\n''; //char str3[]=''lm75 init fail.\n''; //char str9[]=''out of reg conf .\n''; char str4[]=''temp val is.hex..\n''; char st[20]; SystemInit(); init_usart1(); //SENDU(str1); if (!LM75_Init()) { //SENDU(str2); } else { // SENDU(str3); while(1); } SENDU(str4); temp = LM75_ReadReg()>>7; //Temprature register address 0x00 sprintf(st,''temp=%d'',temp); SENDU(st); while(1); } ________________ Attachments : lm75_i2c.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0eI&d=%2Fa%2F0X0000000bbt%2FaGWSKPWwUYJekNo16YRj1KE1wcbqvSs8H_U1UI8PwKo&asPdf=false