ADC 1 problem with STM8S-Discovery
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-26 2:57 AM
Posted on May 26, 2015 at 11:57
Hi,
I have problem with ADC1 conversions on STM8S-Discovery. I have configured the analogic inputs following: PB4 - AN4 PB5 - AN5 PB6 - AN6 unsigned char ADC_Config_INT ( void ) { GPIO_Init(ADC_PORT,ADC_15V_PIN, GPIO_MODE_IN_FL_NO_IT); GPIO_Init(ADC_PORT,ADC_CURR_PIN, GPIO_MODE_IN_FL_NO_IT); GPIO_Init(ADC_PORT,ADC_5V_PIN, GPIO_MODE_IN_FL_NO_IT); /* De-Init ADC1 peripheral */ ADC1_DeInit(); /* Enable EOC interrupt */ ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE); /* Enable conversion data buffering */ ADC1_DataBufferCmd(ENABLE); /* Enable scan mode conversion */ ADC1_ScanModeCmd(ENABLE); /* Init ADC1 peripheral */ /* ADC1 Channel 4 */ ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_4, ADC1_PRESSEL_FCPU_D8, \ ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL4,\ DISABLE); /* ADC1 Channel 5 */ ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D8, \ ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,\ DISABLE); /* ADC1 Channel 6 */ ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_6, ADC1_PRESSEL_FCPU_D8, \ ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL6,\ DISABLE); /* Enable ADC1 */ ADC1_Cmd(ENABLE); return 0; } the interrupt function code is: #define ADC_SAMPLES 8 extern volatile uint16_t ValueCh4[ADC_SAMPLES]; extern volatile uint16_t ValueCh5[ADC_SAMPLES]; extern volatile uint16_t ValueCh6[ADC_SAMPLES]; volatile uint8_t Index = 0; extern uint8_t ArrayEmpty; /** * @brief ADC1 interrupt routine. * @param None * @retval None */ INTERRUPT_HANDLER(ADC1_IRQHandler, 22) { if ( ADC1_GetFlagStatus(ADC1_FLAG_EOC) != RESET ) { ValueCh4[Index] = ADC1_GetBufferValue(4); ValueCh5[Index] = ADC1_GetBufferValue(5); ValueCh6[Index] = ADC1_GetBufferValue(6); // Controlla se ho acquisito un numero sufficiente di campioni if( Index >= ADC_SAMPLES ) { ArrayEmpty = 1; Index = 0; } else{ Index++; } ADC1_ClearFlag(ADC1_FLAG_EOC); } return; } The ''ADC1_GetBufferValue'' function return the value correct the first time only. If I modified the value on pin PB4 for example, continuos at read the previous value. Any idea? Thanks
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-26 3:11 AM
Posted on May 26, 2015 at 12:11
ADC 1 problem with STM8S-Discovery
Are you sure you are in the right forum ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-26 4:52 AM
Posted on May 26, 2015 at 13:52
Sorry!
I was wrong forum!