cancel
Showing results for 
Search instead for 
Did you mean: 

stm32e with USB-232 driver

ng_tengjie
Associate
Posted on January 21, 2011 at 10:11

stm32e with USB-232 driver

3 REPLIES 3
Posted on May 17, 2011 at 14:22

No you probably need to be looking at finding a serial zigbee module. Connect it to one of the serial ports. And write you own driver software.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist II
Posted on May 17, 2011 at 14:22

''I need a USB-RS232 converter to physically connect the dongle''

 

You mean it's a USB dongle?

In that case, you would need to provide a USB Host for it.

As Clive1 says, you would be far better off using a Zigbee module with a UART, SPI, or similar interface...
ng_tengjie
Associate
Posted on May 17, 2011 at 14:22

Thanks for the replies! 🙂 Will search for a dongle with serial interface then..

tj