cancel
Showing results for 
Search instead for 
Did you mean: 

RTC count read after power OFF then power ON with 30 sec delay but RTC running with battery

lakshmikantha85
Associate II
Posted on January 27, 2011 at 14:31

RTC count read after power OFF then power ON with 30 sec delay but RTC running with battery

1 REPLY 1
Posted on May 17, 2011 at 14:23

Perhaps you should consider putting it in STANDBY (ie handle the imminent lose of primary power case), and checking the STANDBY flag when it comes to reinitializing the RTC. There are also flags for the type of reset that occurred, and there are registers within the BKP domain which you could use to flag your own initialization state.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..