cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 CRC - Preload CRC->DR

mfranklin
Associate II
Posted on March 08, 2013 at 10:31

I've stolen some code from Clive's post here <https://my.st.com/a99fbbe2> (Thanks Clive!) and it works great for computing a CRC all at once. In other words, the following function signature.

unsigned long crc32(const unsigned char* buffer, const unsigned int length);

However, I'm porting some zlib/png code and the CRC is calculated incrementally with the following function signature:

unsigned long crc32(unsigned long crc, const unsigned char* buffer, const unsigned int length);

So, I need to be able to preload CRC->DR with the parameter crc. Anyone know how that can be done? #crc32-crc-stm32f4 #crc #crc32
6 REPLIES 6
Posted on March 08, 2013 at 13:14

The hardware is intrinsically capable of doing bursts of 32-bit words, so you could manage a stream so the hardware register is just left to accumulate.If you have multiple streams, and need to save/restore a specific context there is a math trick to advancing the CRC->DR. It's possible to reverse the polynomial and wind the machine backward to arrive at a magic value to get the next state you want.This is a parallel, small table (4-bit) implementation

https://community.st.com/0D50X00009XkZcLSAV

 

You could check if the register is already where you want to save some time. The code foot print of a serial (1-bit) implementation would be a bit smaller at the expense of some speed.

Edit: Fixed DEAD LINK, original post from March 8, 2013

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mfranklin
Associate II
Posted on March 09, 2013 at 06:25

Wow! A link to source code and everything. I thought my question was so obscure it didn't have much of a chance. Thanks, Clive!

Anyway, it's all working great for me now. Here's my source code in case anyone else finds it helpful.

static
const
uint32_t CrcTable[16] = 
{
0x00000000, 0xB2B4BCB6, 0x61A864DB, 0xD31CD86D, 0xC350C9B6, 0x71E47500, 0xA2F8AD6D, 0x104C11DB,
0x82608EDB, 0x30D4326D, 0xE3C8EA00, 0x517C56B6, 0x4130476D, 0xF384FBDB, 0x209823B6, 0x922C9F00 
};
static
uint32_t ReverseCRC32(uint32_t currentCRC, uint32_t desiredCRC)
{
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];
return
desiredCRC ^ currentCRC;
}
uint32_t Compute(
const
uint8_t* buffer, 
const
size_t
length, 
const
uint32_t crc) 
const
{ 
uint32_t byteCount;
uint32_t bitCount;
uint32_t value; 
//Initialize DR
if
(crc == 0)
{
CRC_ResetDR();
}
else
{
//No need to compute Reverse CRC if DR already has the value we need
uint32_t desiredCRC = __RBIT(crc ^ 0xFFFFFFFF); 
//Compensate for STM32F4's CRC32 shift order
if
(CRC->DR != desiredCRC)
{
CRC->DR = ReverseCRC32(CRC->DR, desiredCRC);
}
}
//Do multiples of 4 bytes (32 bits)
byteCount = length >> 2;
while
(byteCount--)
{
value=*((uint32_t *)buffer);
CRC->DR = __RBIT(value); 
//Compensate for STM32F4's CRC32 shift order
buffer += 4;
}
//Do remaining bytes
value = __RBIT(CRC->DR); 
//Compensate for STM32F4's CRC32 shift order
byteCount = length & 3;
while
(byteCount--)
{
value ^= (uint32_t)*buffer++;
for
(bitCount = 0; bitCount < 8; bitCount++)
{
if
(value & 1)
{
value = (value >> 1) ^ 0xEDB88320;
}
else
{
value >>= 1;
}
} 
}
value ^= 0xFFFFFFFF;
return
value; 
//now the output is compatible with windows/winzip/winrar/zlib/libpng
}

Posted on March 09, 2013 at 07:13

Let's just finish up the demo by table driving the bytes

static uint32_t ReverseCRC32(uint32_t currentCRC, uint32_t desiredCRC)

{

static const uint32_t CrcTable[16] = { // For 0x04C11DB7 Reverse Polynomial

0x00000000, 0xB2B4BCB6, 0x61A864DB, 0xD31CD86D, 0xC350C9B6, 0x71E47500, 0xA2F8AD6D, 0x104C11DB,

0x82608EDB, 0x30D4326D, 0xE3C8EA00, 0x517C56B6, 0x4130476D, 0xF384FBDB, 0x209823B6, 0x922C9F00 };

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

desiredCRC = (desiredCRC >> 4) ^ CrcTable[desiredCRC & 0x0F];

return(desiredCRC ^ currentCRC);

}

static uint32_t FastBlockCRC32(const uint8_t* buffer, const size_t length, const uint32_t crc)

{

static const uint32_t CrcTable[16] = { // For 0xEDB88320 Polynomial

0x00000000,0x1DB71064,0x3B6E20C8,0x26D930AC,0x76DC4190,0x6B6B51F4,0x4DB26158,0x5005713C,

0xEDB88320,0xF00F9344,0xD6D6A3E8,0xCB61B38C,0x9B64C2B0,0x86D3D2D4,0xA00AE278,0xBDBDF21C }; // sourcer32@gmail.com 

while(length--)

{

crc = crc ^ (uint32_t)*buffer++;

crc = (crc >> 4) ^ CrcTable[crc & 0x0F];

crc = (crc >> 4) ^ CrcTable[crc & 0x0F];

}

return(crc);

}

uint32_t Compute(const uint8_t* buffer, const size_t length, const uint32_t crc)

{

uint32_t byteCount;

uint32_t value;

//Initialize DR

if (crc == 0)

{

CRC_ResetDR();

}

else

{

//No need to compute Reverse CRC if DR already has the value we need

uint32_t desiredCRC = __RBIT(crc ^ 0xFFFFFFFF); //Compensate for STM32F4's CRC32 shift order

value = CRC->DR;

if (value != desiredCRC)

{

CRC->DR = ReverseCRC32(value, desiredCRC);

}

}

//Do multiples of 4 bytes (32 bits)

byteCount = length >> 2;

while(byteCount--)

{

value=*((uint32_t *)buffer);

CRC->DR = __RBIT(value); //Compensate for STM32F4's CRC32 shift order

buffer += 4;

}

//Do remaining bytes

value = __RBIT(CRC->DR); //Compensate for STM32F4's CRC32 shift order

value = FastBlockCRC32(buffer, length & 3, value);

value ^= 0xFFFFFFFF;

return value; //now the output is compatible with windows/winzip/winrar/zlib/libpng

}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
matthijs
Associate
Posted on August 18, 2014 at 18:03

Assuming you just want the result and don't specifically need to put the CRC calculator in a specific state, you don't need any tables to deal with initial state or leftover bytes:

My apologies to people allergic to C++, and please beware of the inversion in my definition of read().

struct

crcc {
/*00*/

io_u32 dr;

//r>

/*04*/

u8 idr;

//rw

/*08*/

io_u32 cr;

//-x

u32 rbit( u32 x ) {
u32 y;
asm(

'' rbit %0, %1''

:

''=r''

(y) :

''r''

(x) );
return

y;
}
void

reset() { cr = 1; }
void

write( u32 data ) { dr = rbit( data ); }
u32 read() {

return

~rbit( dr ); }
u32 calc( u8 data, u32 crc ) // single byte
{
crc = ~crc ^ data;
reset();
write( ~( crc << 24 ) );
return

( crc >> 8 ) ^ read();
}
u32 calc(

size_t

nwords, u32 wdata[], u32 crc = 0 ) // wordwise
{
if

( nwords == 0 )
return

crc;
reset();
write( wdata[0] ^ crc );
for

(

size_t

i = 1; i != nwords; i++ )
write( wdata[i] );
return

read();
}
u32 calc(

size_t

nbytes, u8 data[], u32 crc = 0 )// general
{
if

( nbytes >= 4 ) {
// process 0-3 bytes to make pointer word-aligned
size_t

align = -(size_t)data & 3;
nbytes -= align;
while

( align-- )
crc = calc( *data++, crc );
// process bulk of data
size_t

nwords = nbytes >> 2;
crc = calc( nwords, (u32 *)data, crc );
data += nwords << 2;
nbytes &= 3;
}
// leftover bytes
while

( nbytes-- )
crc = calc( *data++, crc );
return

crc;
}

};

This still has a plenty of room for optimization. For example, CRCing 2 or 3 bytes can be done with a single reset/write/read sequence instead of one per byte, e.g.

u32 calc( u16 data, u32 crc )
{
crc = ~crc ^ data;
reset();
write( ~( crc << 16 ) );
return

( crc >> 16 ) ^ read();
}

Also, if you want to perform a new calculation but still know the current state of the CRC engine (because you've just read the data register anyway) you can avoid a reset since

u32 old = read();
reset();
write( foo );

is equivalent to

u32 old = read();
write( foo ^ old );

I'll leave the microoptimizations as an exercise for the reader ;-)
mattreed9
Associate III
Posted on July 21, 2016 at 18:12

This would be awesome if it worked.

I seems to return the exact same values as when I set the HW CRC to InputInversion = WORD and OutputInversion = Enabled.

Which are wrong.

Am I setting the HW CRC up wrong? I have (after adding this code) set InputInversion to NONE and OutputInversion to Disabled.

-Matt

**** CORRECTION ****

It DOES work!  My Linux sample code was passing len = 1 to the crc32 routine, but len is number of bytes, not number of uint32's.  This code worked, the Linux code was wrong.

This is also seen on the on-line CRC calculators (that's how I first noticed it).  If you enter 0x01 you get one value, if you enter 0x00000001 you get another answer.  That's because the on-line calculators determine the number of bytes based on the length of the number you type.

Thank SO MUCH CliVE!!!

-Matt

Posted on July 21, 2016 at 18:30

This would be awesome if it worked.  I seems to return the exact same values as when I set the HW CRC to InputInversion = WORD and OutputInversion = Enabled.

 

Me thinks you are not using an STM32F4 part... It only has fixed and inflexible 32-bit operation.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..