cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042K6T6 ADC Problem

danielblesener9
Associate II
Posted on October 31, 2014 at 21:24

I have a strange problem. I use the code below on the STM32F05 series and it works just fine. Transfer it to the STM32F072 and it does not work. When applying voltage to any given port, the ADC readings change on multiple ports. Voltage reference is stable. Any idea why this would happen?

  //Use the follwing code for interrupts for DMA tranfer complete interrupt and half tranfer interrupt complete. 

  //NVIC_InitTypeDef NVIC_InitStructure;

  // Enable and set DMA1_Channel1 Interrupt */

  //NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;

  //NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;

  //NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  //NVIC_Init(&NVIC_InitStructure);

  // Enable DMA1 Channel1 Half Transfer and Transfer Complete interrupt 

  // DMA_ITConfig(DMA1_Channel1, DMA_IT_HT, ENABLE);

  // DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);

  /* GPIOA Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  GPIO_InitTypeDef GPIO_InitStructure;

  /* Configure ADC Channels as analog input - might conflict */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

  TIM_OCInitTypeDef TIM_OCInitStructure;

  ADC_InitTypeDef ADC_InitStructure;

  DMA_InitTypeDef DMA_InitStructure;

 

  /* ADC1 DeInit */

  ADC_DeInit(ADC1);

 

  /* ADC1 Periph clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_TIM1, ENABLE);

 

  /* DMA1 clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);

 

  /* TIM2 Configuration */

  TIM_DeInit(TIM1);

 

  /* Time base configuration */

  TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);

  TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz, from 48 MHz

  TIM_TimeBaseStructure.TIM_Period = 500 - 1; // 2 KHz

  TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

 

  /* Output Compare PWM Mode configuration */

  TIM_OCStructInit(&TIM_OCInitStructure);

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; /* low edge by default */

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0x01;

  TIM_OC4Init(TIM1, &TIM_OCInitStructure);

 

  /* TIM1 enable counter */

  TIM_Cmd(TIM1, ENABLE);

 

  /* Main Output Enable */

  TIM_CtrlPWMOutputs(TIM1, ENABLE);

 

  /* DMA1 Channel1 Config */

  DMA_DeInit(DMA1_Channel1);

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;

  DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&RegularConvData[0];

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

  DMA_InitStructure.DMA_BufferSize = SAMPLES;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

  DMA_Init(DMA1_Channel1, &DMA_InitStructure);

 

  /* DMA1 Channel1 enable */

  DMA_Cmd(DMA1_Channel1, ENABLE);

 

  /* ADC DMA request in circular mode */

  ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular);

 

  /* Enable ADC_DMA */

  ADC_DMACmd(ADC1, ENABLE);

 

  /* Initialize ADC structure */

  ADC_StructInit(&ADC_InitStructure);

 

  /* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits  */

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

  ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;

  ADC_InitStructure.ADC_ExternalTrigConv =  ADC_ExternalTrigConv_T1_CC4;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;

  ADC_Init(ADC1, &ADC_InitStructure);

 

  /* Convert the  ADC_Channnel_0  with 7.5 Cycles as sampling time */

  ADC_ChannelConfig(ADC1, ADC_Channel_0 , ADC_SampleTime_239_5Cycles);

 

  /* Convert the  ADC_Channnel_1  with 7.5 Cycles as sampling time */

  ADC_ChannelConfig(ADC1, ADC_Channel_1 , ADC_SampleTime_239_5Cycles);

 

  /* Convert the  ADC_Channnel_2  with 7.5 Cycles as sampling time */

  ADC_ChannelConfig(ADC1, ADC_Channel_2 , ADC_SampleTime_239_5Cycles);

 

  /* Convert the  ADC_Channnel_3  with 7.5 Cycles as sampling time */

  ADC_ChannelConfig(ADC1, ADC_Channel_3 , ADC_SampleTime_239_5Cycles);

 

  /* Convert the  ADC_Channnel_4  with 7.5 Cycles as sampling time */

  ADC_ChannelConfig(ADC1, ADC_Channel_4 , ADC_SampleTime_239_5Cycles);

 

  /* ADC Calibration */

  ADC_GetCalibrationFactor(ADC1);

 

  /* Enable ADC1 */

  ADC_Cmd(ADC1, ENABLE);

 

  /* Wait the ADCEN flag */

  while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));

 

  /* ADC1 regular Software Start Conv */

  ADC_StartOfConversion(ADC1);

  

  return;
1 REPLY 1
danielblesener9
Associate II
Posted on November 03, 2014 at 23:20

Problem solved. Code above works fine. Grounding issues from unstable split supplies.