cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207 Low Power mode options

Barbie
Associate II
Posted on December 13, 2012 at 14:01

I can't fine an example of sleep mode configure. Can someone send me a link?

If I want to active the UART and RTC in low power mode. What is the lower mode option I can use?

#an3430-low-power-mode-stm32f2
1 REPLY 1
Nickname12657_O
Associate III
Posted on December 27, 2012 at 12:33

Hi Strauss,

The following AN3430 may bring you some help, if you still need it ;) 

 

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/APPLICATION_NOTE/DM00033348.pdf

 

Cheers,

STOne-32